Ceramic Capacitors FAQQWhat is the status of the “GA3” (Type GD) “Y3” series, which is a subclass of the “Y” Class capacitors under safety standard IEC60384-14. Since the Safety standard for the “Y3” series, under SEMCO (Sweden) standards has been abolished, will the production of the “GA3 Series (Type GD)” “Y3” capacitors be discontinued?