■Soldering Condition with iron
Pre-heating(60 to 80゚C, 10 sec. min)
|
Component Part
|
Temperature (゚C)
|
Time (sec. max.)
|
①
|
Electrode
|
320 to 350
|
0.5
|
②
|
Metal Plate
|
410 to 450
|
3.0
|
■ Position
The farthest position from the center of the Piezoelectric Diaphragm is recommended, because the soldering point works as a load that restricts its oscillation.
The lead wire should also be as fine as possible. (Ex: AWG32).
(Reference)
Piezoelectric Sound Components Application Manual
Related FAQs
Most people who viewed this page also referred to the following pages.
Q.
Are there any points to be aware of handling diaphragm with lead wires?