The reference FCC certification is provided. Customer can use this certification if they use the same (or similar) antenna.
The CE certification needs to be done on the final product, not the module. Hence, customers will need to handle this over their end. However, Murata can provide the data to assist.
Return to LoRa Module Page
Back to LoRa FAQ List