CERALOCK have two built-in load capacitors inside, C
L1 at input side and C
L2 at output side. Capacitance value of C
L1 and C
L2 are not completely equal.
Oscillation frequency : Fosc is approximated by following formula.
When CERALOCK is mounted in opposite side, positions of built-in load capacitors C
L1 and C
L2 are switched. Because of the difference of capacitance value of C
L1 and C
L2, frequency correlation occur.
Related FAQs
Most people who viewed this page also referred to the following pages.