World's First SAW Filter/Power Amplifier/Magnetic Stabilizer in One Package: Mobile Phone Transmission Module to Be Marketed

World's First SAW Filter/Power Amplifier/Magnetic Stabilizer in One Package: Mobile Phone Transmission Module to Be Marketed

9/13/2011

Murata Manufacturing Co., Ltd.

President/ Statutory Representative Director: Tsuneo Murata

Overview

Murata Manufacturing Co., Ltd. has developed and begun mass production on a mobile phone transmission module.

The module is the world's first to integrate the peripheral parts, mainly a SAW filter*1, power amplifier*2 and magnetic stabilizer*3, into one package. It offers a low and compact form as well as extremely high stability under load fluctuation. These characteristics will help to make mobile phone design simpler and less labor intensive, while limiting fluctuation in characteristics when the mobile phone usage environment changes.

The module will be on display at CEATEC JAPAN 2011 at Makuhari Messe in Chiba Prefecture, October 4-8.

Background

Recent years have seen a growing number of frequency bands supporting 3G networks. The more complicated circuit board layouts have made it more difficult to achieve compact design. Murata Manufacturing developed the module putting the SAW filter, power amplifier and magnetic stabilizer in one package to meet the need for compact modules that do not require matching.

Features

  • With the SAW filter, power amplifier and magnetic stabilizer in one package, the high degree of integration reduces the footprint
  • Successful mass production of a magnetic stabilizer based on isolator technology enables isolator-free design and keeps module height low
  • Shorter set design times
  • Enables design without matching to SAW duplexer
  • Controls fluctuation in such characteristics as bit error rate when antenna impedance changes, making it possible to maintain communications quality without depending on antenna status
  • Bands: Supports Band 5 (BC 0) , Band 1 (BC 6) , Band 25 (BC 14) , Band 13
    *Frequency is currently being further expanded

Terminology

*1 SAW filter: An element using the characteristics of piezoelectric bodies to get an electrical signal of a certain frequency band
*2 Power amplifier: A semiconductor that amplifies a high-frequency signal in a mobile phone, etc. when that signal is transmitted
*3 Magnetic stabilizer: This load-resistant element is a magnet used in an isolator. It controls fluctuation in characteristics caused by changes in impedance (deviation of antenna characteristics) that occur when the user's hand, metal or other material nears the antenna.

Applications

Mobile phones, smartphones

Part Number

  • HFQPRAPCA-064
  • HFQPRAPCA-065
  • HFQPRAPCA-066

Electrical Performance

Representative Characteristics

Part Number: HFQPRAPCA-064

Main Characteristics (Gain, Consumption Current)

Main Characteristics (Gain, Consumption Current)

ACPR (CDMA2000 1x)

ACPR (CDMA2000 1x)

UMTS

ACLR (UMTS R99, HSUPA)

ACLR (UMTS R99, HSUPA)

LTE

UTRA (BW 10MHz RB50 16QAM)

UTRA (BW 10MHz RB50 16QAM)

External Size

6.6mm (typ) x3.8mm (typ) x1.0mm (MAX)

Production

Mass production began at Komatsu Murata Manufacturing Co., Ltd. in July 2011

Sample Price

500 yen per unit


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com