Murata announces highly efficient combined 3-phase PFC and DC-DC converter for data centre applications

PFC converter with 3-phase AC input support


Murata Manufacturing Co., Ltd.

President/Statutory Representative Director: Tsuneo Murata
Murata today announced two products that are designed to improve power conversion efficiency in large data centre environments. These complementary products are a 5kW PFC converter with 3-phase AC input and a matching high input voltage 1,200 Watt DC-DC converter. High voltage direct current (HVDC) power supply solutions are increasingly becoming popular as a way to power large server racks and datastorage equipment in the most energy efficient means possible. These two new products achieve this while meeting the restrictions placed on reducing higher harmonics to a minimum. 

The PFC converter, model number MPA9535, operates from a high-line 3-phase 480 VAC input and provides a 380 VDC output. The converter ensures that the power factor correction is a close as possible to unity thus ensuring that efficiency is as high as possible. Typical power conversion efficiency of the MPA9535 is up to 96%. The matching MPA9512 DC-DC converter is fed directly from the MPA9535 and has two DC outputs. The main output is 12.12 VDC and a standby +5 VDC output is also provided. This stage of power conversion achieves a typical efficiency of 95.2%.

Designed for use in standard 19-inch server racks, the two units combined occupy a 4U footprint.
Mass production will commence during 2015.
Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at