| 1 | We make an effort in the reduction of the carbon dioxide discharge positively. We carried out the economy in power consumption of illumination / the office appliance with all the members. In addition, I performed the update of a utility / the air conditioner, the change of the production method of construction. As a result, about 21% reduced a carbon dioxide discharge by the ratio in a sales amount basic unit against FY1990. |