murata EnglishChineseJapanese
地区
GlobalNorth AmericaEurope


会长、社长致辞
一目了然的村田
以数字看村田
特辑 CSR管理与利益相关者的经济关系
环境与村田 人与村田 第三方评论
编者的话
Guideline Comparison Sheet
CSR Report
按据点区分的CSR 报告
CSR Report by business site Back to the List
Toyama Murata Manufacturing Co., Ltd.
据点首页 环境目标与实际成绩 环保话题 社会性活动话题 环境数据

No Targets for fiscal 2006 Results from fiscal 2006 Achievement
1 Reduction of PFC emission
To make PFC using for the adjustment of the product GWP 28,300t.
GWP 26,248t
2 Reduction of hazardous substances
The reduction of the quantity of consumption part disposal : 17% reduction (BM: FY2003)
The reduction of the VOC discharge : Less than discharge 44,160kg
32% reduction
The amount of discharge: 42,192kg
3 The development of the small article
① Development progress rate (article A) : 100%
② Development progress rate (article B) : 100%
③ Development progress rate (article C) : 90%
④ Development progress rate (article D) : 10%
0%
Development cancellation by the business-related point of view
70%
(We needed time for problem solution about the reliability evaluation)
90% (We needed time for problem solution about the reliability evaluation)
10%
×
4 Promotion of the green supply
We carried out the inspection of all four suppliers whom we intended for and confirmed a thing without the problem to them.
5 Reduction of the electricity consumption
Production amount basic unit 12.6% reduction (BM FY2000)
15.3% reduction
6 Reduction of waste emission
Sales amount basic unit 35% reduction (BM FY2000)
25.5% reduction
×
7 Reduction of groundwater consumption
500km3 reduction
218km3 reduction
×
8 Promotion of the local contribution
Periodical neighboring local cleaning
The snow removing of the neighboring sidewalk
Enforcement as scheduled
There was not the opportunity of the snow removing for a mild winter.
* Achievement
    Criteria
Achieved
× Not Achieved

Top of page