murata EnglishChineseJapanese
地区
GlobalNorth AmericaEurope


会长、社长致辞
一目了然的村田
以数字看村田
特辑 CSR管理与利益相关者的经济关系
环境与村田 人与村田 第三方评论
编者的话
Guideline Comparison Sheet
CSR Report
按据点区分的CSR 报告
CSR Report by business site Back to the List
Murata Manufacturing Co., Ltd. Yasu Plant
据点首页 环境目标与实际成绩 环保话题 社会性活动话题 环境数据


1 The introduction of high efficiency gas engine cogeneration facilities
We introduced the gas engine cogeneration facilities of the high efficiency. As for these facilities, we can generate electricity about 20% of the electricity demand, and the exhaust heat to occur can use air conditioning warm water and process steam.
It came to be under CO2 discharge by reduction hereby in 1,660t / year.

2 The remodeling of the lead closed system
The waste fluid which occurred from a lead closed system held about 16% of waste with our plant.
We did water confirmation of the water which we treated and remodeled the institution to be able to discharge it into the sewer.




Top of page