Global / MURATA MANUFACTURING CO., LTD.
Help

Mobile Communications

Between you and that somebody

Enter the New Mobile Era with Murata Technology

More than two billion people around the world now own mobile phones, and the number is rising rapidly. The third-generation of communication systems, such as UMTS, W-CDMA and CDMA 2000, are being replaced by the next-generation systems including 3.9G, 4G and WiMAX.In addition to phone call, e-mail, and digital camera features, modern cellular phones serve as navigation consoles and e-wallets. They also enable quick download of large-volume data.Murata will remain at the forefront of fast-evolving mobile technology.

Top of Page

Mobile Technology Gets Streamlined

Lately, most mobile phones no longer have whip antennas. This has been made possible by advancements in the technology used to integrate the antenna in the handset, and our ceramics chip antennas are greatly contributing to this trend. Murata’s new antennas feature a mix of our special materials, design, electrode and multilayer technologies in order to provide optimal reception of a variety of wireless signals. Our antenna lineup, which includes dielectric antennas and multilayer antennas optimized to receive the 800MHz, 1.5GHz, 2.4GHz and other frequencies is playing a major role in making mobile phones even more functionally sophisticated while further reducing their size and thickness.

Chip Dielectric Antennas

Chip Dielectric Antennas

Top of Page

Advancement in Filter Technology is the Key to Downsizing

The filter selects only the necessary frequency from radio signals. Larger number of duplexers dividing the frequency into transmitting and receiving bands tends to be used as mobile phone system becomes more highly integrated and sophisticated. Consequently, those duplexers are required to be smaller and thinner. Murata fulfills these requirements by offering SAW devices and the world’s first filter that employs boundary elastic waves. Our products are indispensable in designing these highly functional, yet stylish and thin phones.

Buried Propagating Layer Acoustic Wave Filter /SAW Filters /SAW Duplexers

Buried Propagating Layer Acoustic Wave Filter /
SAW Filters /
SAW Duplexers

Top of Page

Integrating Both Transmit and Receive Functions of the Mobile Phone with One Component

Signals passing through the antenna contain much interference. The mobile phone consists of complex circuits to handle various functions, including a filtering function to eliminate noise and a switching function to switch between transmitting and receiving. Multilayer modules have been conceived in order to integrate all these functions in a single component. Several ceramic sheets that can be co-fired at low temperatures are laminated together to form passive components such as inductor (coils), capacitors and RF-passive components. Semiconductive components and other components are mounted on the surface of the ceramic substrate.

SWITCHPLEXER®

SWITCHPLEXER®

Top of Page

Wide Array of Communication Modules

Murata develops a broad range of RF modules for mobile phones and other mobile equipment. Our lineup of modules for Bluetooth® (a new method for short range wireless communication), includes Blue Device®, an RF module dedicated for RF circuits, and Blue Module®, an HCI (Host Controller Interface) module that combines a Blue Device® module with other components, such as baseband signal processing circuits and flash memories. Use of low-temperature, co-fired ceramic multilayer substrates makes both modules the world's smallest in their categories. Murata also offers small high-performance modules for use in car navigation systems, mobile phones and GPS (satellite-based Global Positioning System).

left: Bluetooth®Modules right: GPS Modules

left: Bluetooth®Modules
right: GPS Modules

Top of Page

Murata Products around Us

Contact Us

THE AKIRA MURATA STORY

Home > About MURATA > Technology > Murata Products around Us > Mobile Communications

Help

Global / MURATA MANUFACTURING CO.,LTD.