Murata's integrated production system leads from materials to finished products, allowing accumulation of technological elements such as materials, processing, design, and production technology, as well as supporting software, analysis and evaluation. The foundation for Murata's R&D system is its vertically integrated technological elements. In our integrated production system, all technological elements are sequenced and mutually connected with each other. Specialists representing various fields closely exchange information with each other to seek a common goal; the flexibility and efficiency of this R&D system is Murata's unrivaled strength.
Immediate Focus of Technological Assets at Breakthrough Points
Reducing the chip by 0.1 mm, increasing the bandwidth by 1 GHz, developing a new ceramic material-research and development efforts encounter myriad breakthrough point. That is when a wide range of intellectual assets is immediately assembled through Murata's vertical integration of technologies.

Tackling R&D themes with optimal team formation
Vertical integration of technologies requires teamwork beyond organizational boundaries. All R&D teams in Murata are intersectional. We challenge our development themes by optimally utilizing all technological elements accumulated in the company. For especially important projects, selected members temporarily leave their own departments to dedicate themselves to the project and conduct research and development intensively. We always optimize our development teams to flexibly deal with the development phase or a change in the market. This sort of flexibility helps Murata's research and development system to immediately answer current demands.
We tackle new challenges in thin film process technology and micro-fabrication technology in our clean room.
The STEP education program for engineers, and the university alliance program in existence since foundation
Since Murata's foundation for research and development is vertically integrated technologies, every specialist is required to be well versed in other fields. Murata's original training program, STEP (Strategic Technology Program) is intended to promote such learning opportunities for specialists. To construct a high-level technological foundation, we aim to further strengthen fundamental technologies through free small group activities. Cutting edge technical information is disseminated horizontally in the company, and at the same time technological information accumulated within the company is taught through lectures. We also form alliances with external research institutes, including universities. For Murata, which has developed applications for unexplored barium titanate with the cooperation of a Kyoto University research team since its foundation, alliances with universities are another valuable intellectual asset. We value mutual technological cooperation between Murata and academia. Technologies nurtured through such alliances are shared among many specialists in Murata through the STEP program.
Cooperation with the R&D division was fortified at the Murata headquarters to increase efficiency in R&D and commercialization of new products. A new complex, which is currently under construction, will help to firm up our business foundation and further expand operations.
The base for research and development of production technologies, electronics material technologies focused mainly on ceramics, and thin film processing technologies.
The base for development of communication and sensor functional modules for next generation systems. They are equipped with one of the largest electromagnetic anechoic chamber.
Organization