| No |
Targets for fiscal 2006 |
Results from fiscal 2006 |
Achievement |
| 1 |
Reduction of Chemical substances
2% decrease compared to the previous fiscal year
Target : 20.2 (kg/MPC) |
Result : 25.3 (kg/MPC)
The production required amount per 1 increased by article introduction of the large-scale size |
× |
| 2 |
Reduction of CO2 emission
2% decrease compared to the previous fiscal year
Target : 1.87 (t-CO2/M yen) |
Result : 1.90 (t-CO2/M yen)
Increase of the electricity consumption with the injection of the new kind, the increase in production, and the kitchen start
Outbreak of the loss (the operation that does not become the production results) by the introduction of the rationalization line
|
× |
| 3 |
Reduction of groundwater 20% decrease compared to FY2003 Target : 71,949 tons (as amount of reduction) |
Result : 70,766 tons
The operative contents review of the cooling tower
A change of the manufacturing method
|
○ |
| 4 |
Reduction of water 5% decrease compared to FY2003 Target : 3,523 tons (as amount of use) |
Result : 3,169 tons
Continuous saving water enforcement |
○ |
| 5 |
Reduction of waste emission
1% decrease compared to the previous fiscal year
Target : 82.0 (kg/M yen)
Rate of Recycle: maintain to 100“ |
Result : 66.7 (kg/M yen)
A metal value thing
The update of facilities
|
○ |
| 6 |
Eco-harmony with the community
①An interesting technical contact classroom for children in the summer vacation
②Azumino Festival / Matsumoto industry Festival
③Activity of periodical cleaning
④Participation to the Alps Hana Kaido
Target : Carry it out as scheduled |
Result : Carried it out as scheduled |
○ |
| 7 |
Tree Planting
Enforcement of the tree planting activity to lead to the making of rich environment
Target : Carry it out as scheduled |
Result : Carried it out as scheduled |
○ |