murata EnglishChineseJapanese
Region
GlobalNorth AmericaEurope


Top Commitment
Recognizing Murata
Murata by the Numbers
Feature CSR Management Economic Relations with Stakeholders
Murata and the Environment Murata and People Third-Party Comments
Editorial Policies
Guideline Comparison Sheet
CSR Report
CSR Report by business site
CSR Report by business site Back to the List
Beijing Murata Electronics Co., Ltd.
Profile Targets and Results Environmental Activities Social Activities Environmental Data

Environmental Data 2007
Energy data
Electricity consumption: 9,332,028 kWh/year
Fuel consumption: 0 kl/year
*The fuel consumption values have been obtained by converting the consumptions of heavy oil, kerosene and fuel gas into the equivalent consumption of petroleum. For this purpose, the conversion coefficient for plants in Japan and overseas is the one mentioned in the regular report per "Law Concerning the Rational Use of Energy in Japan".
Waste volume data
Total waste released: 336.45t/year
Annual mean recycling ratio: 100%
*"Recycling ratio" refers to a ratio of waste (including salable waste) sold or recycled to the total amount released (other than a waste that appears not to be coped with by the efforts of Murata).
Water quality data
The management level is strictly enough to meet the target level.
Item Unit Target level Average Max value
Hydrogen ion concentration(pH)   6-9 7.63 7.72
Suspended Solids(SS) mg/l 80 36.5 37
Chemical Oxygen Demand(COD) mg/l 100 45 56
Biochemical Oxygen Demand(BOD) mg/l 30 8 16
Ammonia nitrogen(NH3-N) mg/l 15 1.29 1.92
Color 80 7 10
*Water quality data are the values measured at the final discharge point.
Air quality data
The management level is strictly enough to meet the target level.
Item Unit Target level Average Max value
Organic matters belonging to hydrocarbon groups other than methane mg/Nm3 120 10.87 19.48
*Air quality data are the values measured at the exhaust point.

Past Environmental Data
FY2006 FY2005

Top of page