Murata’s collaboration with Beta LAYOUT delivers comprehensive UHF Passive RFID starter kit

08/02/2012

Murata and Beta LAYOUT, a company specializing in rapid PCB prototyping services, today announced the launch of an RFID starter kit based on Murata’s MAGICSTRAP® UHF passive RFID devices. Aimed at engineers and developers wishing to quickly learn about and incorporate RFID into their electronics design, the kit comprises a reader/writer board, communication software, two reader antennas and four different kinds of MAGICSTRAP® RFID tag modules. One reader antenna is designed for standard applications where the detection range is up to several metres. The loop antenna is provided for use in hidden applications such as for anti-counterfeiting and brand protection. Using the kit allows engineers to trial the full versatility and flexibility of MAGICSTRAP® RFID devices. Communication over short distances for individual tag connections can be experienced as well as bulk reading of MAGICSTRAP® based PCB tags as necessary in logistics processes. Typical applications for MAGICSTRAP® RFID include any type of electronics application such as mobile phones, industrial control, consumer electronics and test & measurement equipment. Alexander Schmoldt, Business Development Manager, Murata Europe comments, “The combination of Beta LAYOUT’s excellent customer service and their rapid prototyping services makes them a perfect partner for Murata. Beta LAYOUT has a large pan-European customer base. They are a perfect partner for us to deploy our RFID technology into the electronics manufacturing and supply chain across Europe.”

“Murata’s MAGICSTRAP® is exactly the solution we have been waiting for,” says Arne Hofmann, CEO Beta LAYOUT. “Finally it is possible to use RFID on and in a PCB. Our solution to embed the MAGICSTRAP® in a PCB (patent pending) is not something far away in the future but available here and now. Aside from selling it as a service and product to our customers, we will also use it to improve our own processes. We are just at the beginning of a very exciting cooperation.” The basic UHF-RFID starter is available for purchase  from Beta LAYOUT.


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com