Ceramic Capacitors FAQQWhat is the MSL level of the ceramic capacitors?

A
Evaluations performed by Murata revealed the MSL of the chip multilayer ceramic capacitor is 1 and the MSL of the resin mold surface applied type ceramic capacitor (DK1, EVA Series) is 3. Since products compatible to reflow soldering are applicable to MSL, products dedicated to flow soldering, such as parts with leads, are not applicable.

MSL is a JEDEC standard, and is intended for the phenomenon where the cubical expansion generated by the gasification of the moisture included in the product due to the moisture absorption of the product and the reflow soldering during mounting, which results in failures. The level that expresses this risk is the "MSL" (Moisture Sensitivity Level). As the level increases, the risk becomes higher; therefore, it is necessary to prevent moisture absorption when the level reaches 2 or more. For that reason, products of level 2 or higher must go through a baking process at a fixed period, and the tape reel is packaged in an aluminum pack with a desiccant.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.