Inductors FAQQThe wire wound inductor disconnected, what is the cause?

A
In order to focus on the performance, there are portions of the wire wound inductor which are coated with resin.  Even if there is coating, the lead lines are not protected.  For this reason, pay sufficient attention when handling the components, and be careful not to scratch the components with pincettes or etc.  Also, if the board mounted with components is stored in a stack, the corner of the boards will make contact with the components of the other boards and cause wire breakage.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.