Piezoelectric Buzzers FAQQDo Sound Components acquire UL standard certification on flame resistance(UL94)?

A
As a component, they do not acquire UL standard certification, but they are composed of UL standard certified material in the plastic case and the coating of lead wire.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.