NTC Thermistors FAQQ[NC* Series] Why isn't the B constant a negative value?

A

See B constant in the Basic Knowledge . From the thermistor characteristic equation, the resistance value is proportional to the B constant and the temperature 1/T. If the horizontal axis is 1/T, the graph has a positive slope. The B constant is therefore a positive value.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.