They shows frequency marking and EIAJ Monthly Code. Please refer to the following figure.
|
CSTCR_G / CSTNR_G / CSTNE_G / CSTNE_V Series
|
*1:Frequency Marking
The following table shows typical examples of frequency marking.
Regarding other frequency, please refer to each specification or contact us.
Series
|
Explanation
|
Example
|
CSTCR_G/
CSTNR_G
|
We mark the second decimal place of the frequency without a decimal point.
|
6.000MHz→600
|
CSTNE_G
|
We mark the first decimal place of the frequency without a decimal point.
But we replace number with the alphabet when the integer part of the frequency is a 2-digit. 10→X、11→Y、12→Z.
|
8.000MHz→80
10.000MHz→X0
|
CSTNE_V
|
We mark the code as the frequency.There is no regularity.Please refer to specification of components.
|
20.000MHz→E
24.000MHz→J
|
*2:EIAJ Monthly Code
Marking code for manufacturing month & year
|
Note) One cycle (A to z ) : Four years
|
Related FAQs
Most people who viewed this page also referred to the following pages.