Murata to exhibit at OFC 2017

Murata to exhibit at OFC 2017

3/13/2017

We’re pleased to announce that Murata Electronics will be exhibiting at the Optical Fiber Communication Conference® and Exposition, March 21–23, at the Los Angeles Convention Center. Visit us at booth 3152.

See how Murata is shaping the future of optical engines for high-speed network computing.

Murata products and demos featured for optical engine solutions:

Fiber Optical Transceiver – Small optical engine
Murata will show several types of small size optical engine, such as
  • 40Gbps transceiver
  • 56Gbps transmitter/receiver
  • 100Gbps transmitter/receiver
  • 100Gbps transceiver with robust connector function

Murata’s optical module can be installed by SMD reflow assembly process, and optical coupling is done using a simple pluggable connector.

Wireless Optical Transceiver
Murata will demonstrate small size optical wireless transceiver module, which has 10Gbps data transfer capability, compatible for USB3.0/3.1 interface. The module contributes to the connector-less high speed data transfer among gadgets.

µDC-DC converter
Murata will display a small case size, low EMI noise µDC-DC converter module that integrates a power inductor in the ferrite multilayer substrate. We will also exhibit a Point-of-Load module for system boards.

Crystal
Murata’s advanced package technology allows for balanced competitive performance and cost.


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com