Murata' s Ceramic Capacitor for Power Electronics Wins an Elektra Award

Murata’s Ceramic Capacitor for Power Electronics Wins an Elektra Award

1/13/2010

Murata Manufacturing Co., Ltd.
President/ Statutory Representative Director:
Tsuneo Murata

Production of this product has stopped.
Contact Murata for inventory availability and
possible alternative products.

Overview

EVC series capacitor for power electronics, developed by Murata Group (hereafter called Murata), has been awarded an Electra Award in the “Passive & Electromechanical Product of the Year” category.

Excellent technologies and innovations in the field of electronics are awarded at the Elektra Awards hosted by Electronics Weekly, a British technological magazine catering to the largest number of subscribers in the industry. The Elektra Awards are given to products representing excellent European technologies and innovations in the field of electronics in 15 categories annually.

This year, Murata’s ceramic capacitor for power electronics won an award in the “Passive & Electromechanical Product of the Year” category.

Murata will continue to provide innovative products as an innovator in the electronics industry.

Details of EVC series capacitor for power electronics

Details of EVC series capacitor for power electronics

EVC is a monolithic ceramic capacitor series specialized for power electronics.
Conventionally, film capacitors and aluminum electrolytic capacitors have been used in power system electric circuits of electric vehicles and hybrid vehicles. Murata developed new elemental technologies to commercialize ceramic capacitors usable in power electronics applications. Replacing conventional capacitors by ceramic capacitors makes equipment smaller and able to handle high currents. EVC series was introduced in KERS (Kinetic Energy Recovery System) used in F1 racecars. Murata intends to widely promote solutions taking advantage of excellent potentials of the EVC series.

Features

  • Can be made smaller than film capacitors and aluminum electrolytic capacitors due to larger capacitance per unit volume.
  Film capacitor Aluminum electrolytic capacitor EVC series
Capacitance per unit volume (μF/c.c.) 1.2 1.9 2.4

(DC630V rated voltage equivalent. Measured for actual usage. In-house comparison.)

  • Less heat radiation and larger allowable ripple current due to low ESR, accommodating high current making it suitable to inverter circuits on-board.
  • Excellent surge suppression due to low ESL

Specification

Dimensions 32.0×40.0×4.0mm
Rated voltage DC200V
Allowable ripple current 25A (r.m.s)
Effective capacitance 38μF (when applying DC150V)
Capacitance 52μF

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com