Murata introduces 03025-size 3-line common mode noise filters for the MIPI C-PHY I/F

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

5/17/2017

This product has been discontinued. (*Updated on Jun 24, 2022)

NFP0NCN Series

Overview

Murata Manufacturing Co., Ltd., has released the NFP0NCN series of 3-line common mode noise filters for the "MIPI*1  C-PHY" high-speed differential interface. Mass production of this new product began in April 2017.

  

Supplementary notes

Currently, the "MIPI D-PHY" is being used as the interface between the camera module and display module of mobile equipment.

Yearly advances in camera resolution have resulted in proportionate increases in the volume of information to be handled. This has led to the development of the MIPI C-PHY next-generation camera serial interface, which is capable of handling the transfer of larger volumes of data even at high speeds.

This C-PHY interface differs considerably from the D-PHY, which has conventionally transferred data over two lines, in that the C-PHY uses three lines to transfer data. However, conventional 2-line common mode noise filters cannot be used with the C-PHY interface because of the larger adverse effect on transmission signals.

For this reason, Murata Manufacturing has applied micro wiring technology using photolithography to join each of the three lines in the development of the "NFP0NCN series" of 03025 inch size (0.85 x 0.65 mm) 3-line common mode noise filters for the MIPI C-PHY interface.

  

Product site URL

Terminology

*1 MIPI: Mobile Industry Processor Interface


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter