Start of Bluetooth® SMART Module Mass Production —LBCA2ZZVZE—

Start of Bluetooth® Smart Module Mass Production —LBCA2ZZVZE—

5/29/2012

Murata Manufacturing Co., Ltd.

President/ Statutory Representative Director: Tsuneo Murata

Overview

Murata Manufacturing Co., Ltd. will mass-produce a Bluetooth® Smart* module that supports the Bluetooth® low-energy standard, starting from June.
This product will be exhibited within the Texas Instruments booth at "Wireless Japan 2012, " which will be held at Tokyo Big Site from May 30.

Background

Bluetooth® low energy (BLE) is an ultra-low power communication technology that enables months to years of operation with a button battery. Widespread application is expected in various fields such as health management, fitness and home networks. In addition, BLE has also been adopted as a communication method by the Continua® Health Alliance, a non-profit organization of leading healthcare and technology industry companies.

BLE is being successively adopted for use in mobile terminals such as smartphones and tablet terminals, and expectations are increasing for BLE as a means of seamlessly connecting mobile terminals with health management devices such as blood pressure meters and bathroom scales, and battery-driven devices such as wristwatches and compact sensors.

For example, data can be collected and managed between mobile terminals and wireless health devices equipped with BLE, enabling health management anytime, anywhere. In addition, devices connected to smartphones and other applications are also expected to expand in the future.

To meet these market needs, Murata has worked to develop a Bluetooth® Smart module that supports the Bluetooth® low-energy standard, and will start mass production from June of this year.

Features

This module will provide powerful support for the network capability of customer devices.

  • All protocol stacks required for Bluetooth® low-energy communication are built in, including various healthcare profiles. The module can also be easily controlled from the 8-bit or 16-bit CPUs often used in embedded devices.
  • Simple commands can be transmitted to the module via a UART interface, enabling easy communication with smartphones and other devices that support Bluetooth® Smart Ready.
  • The module has already acquired various certifications (Radio Act and Bluetooth® Qualification) , helping to greatly reduce customers' development costs.

Applications

Healthcare and fitness devices such as blood pressure meters and bathroom scales Power-saving devices such as wristwatches and compact sensors Smartphone peripheral devices, etc.

Part Numbers

LBCA2ZZVZE

External Size

20.0 (typ) x 13.0 (typ) x 2.4 (max) mm

Production

Mass production will start from June at Komatsu Murata Manufacturing Co., Ltd.

Terminology

*Bluetooth® Smart : This indication is for devices that support Bluetooth® low energy, which is the low-power-consumption version of Bluetooth®. Bluetooth® and Bluetooth® low energy are close-range wireless communication systems that use license-free 2.4GHz band radio waves.

*Bluetooth® standards are prescribed by the Bluetooth Special Interest Group (SIG) .


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com