Murata Manufacturing Co., Ltd. has introduced the DFE18SBN_E0 series of Metal Alloy inductors for the power supplies of mobile devices such as smartphones. This series offers the world’s smallest Metal Alloy power inductor, having lower Rdc*1 than former products. This product entered mass production in April of 2017.
As mobile devices continue to implement higher density and greater performance, the market requires a small-sized power inductor that can support a large current. For this reason, Murata has made unique improvements to the metal magnetic material, thereby reducing the Rdc in comparison to the former DFE18SA series, while maintaining DC superimposition characteristics. (The DFE18SA series has Isat*2 =2.0A, Rdc=144mΩ@1uH, while the new DFE18SBN_E0 series has Isat=1.9A, Rdc=120mΩ@1uH.)
*January 9th、 2018 Changed specifications of DFE18SBN_E0
*1 Rdc: DC resistance
*2 Isat: Rated current based on change in inductance
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com