Murata develops world's smallest combined proximity and illuminance sensor

Illuminance sensor

5/8/2014

Murata Manufacturing Co., Ltd.

President/Statutory Representative Director:
Tsuneo Murata
Murata today announced what it believes to be the world's smallest combined proximity and illuminance sensor. The surface mounted LT-1PA01 device measures just 3.05×2.10×1.10 mm and integrates both an optical proximity sensor and an illuminance sensor. The proximity sensor uses a photoreceptor to measure the distance to an object based on the amount of returned light. Another photoreceptor is used to detect the amount of ambient brightness. Such sensors are widely used in smartphones to darken the screen when the phone is near the user's face during a call or to increase the brightness of the screen's backlight when used outdoor.

The device has an extremely low power profile, consuming only 80µA during proximity sensing. Illuminance sensing angle is +/-45 degrees at 50% and sensing distance is up to 70 mm with gray card. Operating voltage is +3.3 VDC. Communication with the host processor is via I2C serial communications.
Mass production is scheduled to begin in May 2014.


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com