Ultra compact light and low power SMD piezoelectric sounder suits portable health care devices

SMD piezoelectric sounder

6/18/2014

Murata Manufacturing Co., Ltd.

President/Statutory Representative Director: Tsuneo Murata
Murata today announced they have commenced mass production of, what they believe, to be the smallest and lightest surface mount piezoelectric sounder available. Occupying significantly less surface area, and with a combined weight and area reduction of 44% compared to previous Murata products, the PKMCS0909E4000-R1 measures just 9×9×1.7mm and weighs only 160mg.

Sound pressure level output, measured 10 cm from sounder, is better than 65dB when driven with a ±1.5V 4kHz square wave. Maximum peak-to-peak voltage is ±12.5V. Power consumption is typically 0.6mW, which helps preserve battery life in power budget constrained consumer electronic devices. Since the sounder does not use any magnets or coils to create sound it doesn’t generate any electrical noise and therefore has minimum impact on surrounding circuitry.

Typical applications for the PKMCS0909E4000-R1 include blood glucose meters, personal thermometers, camera strobe flash and Bluetooth dongles.


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com