Murata commercializes compact and highly precise crystal units

11/17/2014

Murata Manufacturing Co., Ltd.
President/Statutory Representative Director:
Tsuneo Murata

XRCGB-F-P series (top) and XRCFD-F/XRCMD-F series (bottom)

Overview

Murata Manufacturing Co., Ltd. has developed two new crystal unit*1 products: the 2016-size (2.0 x 1.6mm) XRCGB-F-P series and the 1612-size (1.6 x 1.2mm) XRCFD-F/XRCMD-F series. 
The XRCGB-F-P series has a frequency precision (initial tolerance + temperature characteristics) of ±40ppm, making it the first device of its type to support wireless communication applications used in wearable and mobile devices such as Bluetooth® low energy (BLE) and ZigBee®. The XRCFD-F/XRCMD-F series has a frequency precision (initial tolerance + temperature characteristics) of ±20ppm, enabling support for Wi-Fi and Bluetooth®.

Background

Murata first commercialized a crystal unit in 2009, after jointly developing it with Tokyo Denpa. While Murata’s ceramic resonators remain popular in automotive and consumer applications, the introduction of the new crystal unit allowed Murata to expand into the hard disk drive (HDD) and solid state drive (SSD) storage market, where higher precision is required. 
The newly commercialized XRCGB-F-P series employs a resin sealing method and delivers even higher precision than its predecessors, making it the first crystal unit to support certain wireless communication applications (devices equipped with BLE or ZigBee®).
The 1612-size (1.6 x 1.2mm) XRCFD-F/XRCMD-F series is a smaller version of the 2016-size (2.0 x 1.6mm) XRCGD series crystal unit employing the alloy fusion sealing method and will contribute to the realization of more compact mobile devices and wireless communication modules.

Features

Achieves high precision due to high-grade quartz crystal components provided by Tokyo Denpa.
Murata’s proprietary packaging technology, unavailable in previous crystal units, enables superior quality and cost performance, and is suitable for mass production. At the same time, it allows superior miniaturization, which enables higher mounting density and thinner products, trends that can be expected to accelerate advancement in the field.
RoHS-compliant and lead-free (phase 3).
Supports lead-free solder mounting.
 

Applications

Wireless devices (mobile phones, Wi-Fi/Bluetooth®, BLE, ZigBee®, NFC)
Wired interface components (Ethernet, USB2.0/3.0)
Imaging devices (TV, LCD, Programmable Display)
PC peripheral storage devices (HDD, SSD, ODD)
Industrial equipment (PLC, Inverter, Servo Amp, Servo Motor)
Processors (CPU, MPU, DSP)
Medical and health management devices


Part number

XRCGB-F-P series
Examples: XRCGB24M000F2P00R0 (24MHz)
                    XRCGB32M000F2P00R0 (32MHz)

XRCFD/XRCMD-F series
Examples: XRCFD26000FYQ000 (26MHz)
                    XRCMD37M400FYQ00R0 (37.4MHz)


Characteristics

Thermal characteristics of XRCGB24M000F2P00R0

Thermal characteristics of XRCGB24M000F2P00R0


Thermal characteristics of XRCMD37M400FYQ00R0

Thermal characteristics of XRCMD37M400FYQ00R0


Electrical characteristics

Item

Specifications

XRCGB-F-P series

XRCFD-F series

XRCMD-F series

Size

2.0 x 1.6 x 0.7mm

1.6 x 1.2 x 0.35mm

1.6 x 1.2 x 0.33mm

Frequency

24 to 27.12 / 30 to 32MHz

24 to 31.999MHz

32 to 48MHz

Freq. Tolerance

±40ppm
(int.: ±20ppm / temp.: ±20ppm)

±20ppm
 (overall)

Operating Temp.

-30 to 85℃


External size

XRCGB-F-P series

XRCGB-F-P series

XRCFD/XRCMD-F series

 XRCFD/XRCMD-F series

Production

XRCGB-F-P series: Mass production underway since September 2014 at Toyama Murata Manufacturing Co., Ltd.
XRCFD/XRCMD-F series: Mass production underway since April 2014 at Toyama Murata Manufacturing Co., Ltd.


Terminology

* Crystal unit: An electronic component that oscillates at a specific frequency that utilizes the piezoelectric properties of quartz crystal. It can generate high precision signals and is used as the source of clock signal for digital circuits.


About Murata

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com