Lead Attaching Technology

Lead Attaching Technology
Chip components which can be mounted on a surface are main stream for passive components as represented by capacitors. However, even in areas where chip components can be used, components where lead wires are attached to Murata's chip components are purposefully used in many cases, due to the mounting convenience of the customer and other special circumstances. The lead attaching technology is introduced in the following.
Murata developed and offers new components with leads, as one of the solutions to respond to the "troubles of customers which cannot be handled by chip components".

Murata Icon X Leaded Products - New Needs and New uses-

Murata Icon X Merits of Lead Attaching

Murata Icon X Summary of Lead Attaching Technology

Murata Icon X Examples of Lead Attaching