Supercapacitors FAQ

Quality/Reliability

Is there any regulation on transportation?

According to 54th Edition of IATA Dangerous Goods Regulations effective from January 1, 2013, Electrical Double Layer Capacitor (EDLC, Supercapacitor) with an energy storage capacity greater than 0.3Wh is treated as dangerous goods and introduced as UN3499 in Class 9.
However, an energy storage capacity of each Murata's supercapacitors is not greater than 0.3Wh. Therefore, Murata's supercapacitors are not covered by this regulation.