Ceramic Capacitors FAQ

Characteristics

What is the temperature character of capacitor's capacitance?

Generally, the capacitance of a capacitor varies according to the working temperature. If the variation of the capacitance is small, the temperature characteristics are good, while if the variation is large, the temperature characteristics are poor. When using capacitors in electronic equipment where the working temperature is high, such as in the engine compartment of an automobile, or in a cold region, such as the South Pole, it is necessary to carry out design that takes into account the conditions of the working environment.

For more details: