Ceramic Capacitors FAQ

Configurations/Material

What is the mechanism of Chip Multilayer Ceramic Capacitors?

A multilayer ceramic capacitor is completed as a chip, mainly through the following eight forming processes.

The structure of the most basic type of capacitor for storing electricity consists of a dielectric sandwiched between two electrodes. A multilayer ceramic capacitor consists of multiple layers of this basic structure stacked on top of each other to enable a greater charge to be stored.

For more details: