Inductors FAQ

How to Use

If a lower inductance is required, there is a method to create this by the board pattern. Will inductors with low inductance no longer be used in the future?

If the inductor is structured on the board, variations will occur in the performance due to the variations in the processing accuracy of the board, or the materials.  On the other hand, since all the inductors used as components are inspected at the time of shipment, variations in the performance is extremely low, and stable performance can be acquired.  For this reason, we believe that inductors used as components will continue to be used.