Trimmer Potentiometers FAQ

Precautions on Using

Can the rotor and adjustment shaft be thread-locked after adjustment?

The only products which can be thread-locked are hermetically sealed products whose wiper and resistive element are not exposed.

Use thread-locking adhesive which does not contain substances that can corrode metals, such as chlorine and sulfur. When using thread-locking adhesive, carefully evaluate its performance on an actual potentiometer.