Trimmer Potentiometers FAQ

Precautions on Using

Can I coat the product with a moisture-proofing agent, or the like?

As with thread locking adhesive, you can apply a moisture-proofing agent only to a hermetically sealed product.

Likewise, use a moisture-proofing agent which does not contain substances that are likely to corrode metals, such as chlorine and sulfur.

When using a moisture-proofing agent, carefully evaluate its performance on an actual potentiometer.