AMR Sensors FAQ

Characteristics

What is sensitivity?

The magnetic field strength at which the AMR sensor is switched on or off. The magnetic force at which the AMR sensor is switched on with an increase in magnetic field strength is referred to as switch-on sensitivity (Hon). Conversely, the magnetic field strength at which the sensor is switched off with a decline in magnetic field strength is called switch-off sensitivity (Hoff).