AMR Sensors FAQ

Characteristics

What is Operating temperatures?

Indicate the temperatures at which the AMR sensor can operate. Note that the operating temperature range varies depending on the product. 
The magnetoresistive element, which forms the core of the AMR sensor, also changes its resistance value depending on temperature. Note that changes in resistance value may cause changes in switch-on and switch-off sensitivity.