Inclinometers FAQ

Operating Circuit

Does the inclinometer SCA61T-FAHH1G have a single pole frequency response?

Yes, SCA61T-FAHH1G has a single pole frequency response. The frequency response of SCA61T-FAHH1G is 8-28 Hz. In addition, the internal ASIC has a 400 Hz low-pass filter.