Inclinometers FAQ

Characteristics

What is the stability of offset calibration accuracy in the SCA61T inclinometer?

Maximum offset calibration error in room temperature is ± 5mg and typical value is ± 2mg (stable) and typical drift is 1mg after 500 hours of having power connected to the inclinometer. Non-repeatability (hysteresis) is 0.25mg when cycling temperature.