Gyro Sensors FAQ

Characteristics

If the max accelerometer cross-axis sensitivity is ± 5%, what is the angle between the direction of measurement (z axis) and the primary axis of sensitivity?

± 5 % cross-axis sensitivity corresponds to approx. 2,8° mounting error. Angle between secondary axis (z-axis) and primary axis (x-axis) is 87,2°.