Inclinometers FAQ

Characteristics

Is the analog output capable of higher resolution than the SPI interface?

Yes, the resolution of the analog output is higher than the digital one. The analog resolution is limited by the output noise density of SCA61T. The noise is 15 µg/√Hz and it yields the following resolutions: 0 - 0.1Hz=>resolution 5 µg, 0 -1 Hz=> resolution 15 µg, 0 - 10 Hz=>resolution = 50 µg, 0 - 30Hz=>resolution is 80 µg