Inclinometers FAQ

Characteristics

In the SCA61T Series, the digital output has an 11 bit resolution. In the SCA 103T the resolution is 12 bits? Is this correct?

The effective digital output resolution of the SCA103T is really 12 bits. This is due to its X-X sensor configuration and the use of the two channels in differential mode. This is how the effective resolution of 12 bits can be achieved.