Shock Sensors FAQ

Characteristics

Can the strength of shock be determined?

The output of shock sensor is the amount of charge proportional to the magnitude of applied shock, it is impossible to determine the intensity alone. However the magnitude of shock is detectable by adding peripheral circuit (amplifier and comparision circuits). It is necessary to check and adjust output through actual set by defferent vibration trasmission depending on mount position or around circuit devises.