Ultrasonic Sensors FAQ

Characteristics
Waterproof type/Open-Structure type/High-Frequency type

Is it possible to detect an object that is placed behind a film?

It depends on the thickness of the film and the distance to the object. It may be possible if the film is thin enough for the ultrasonic wave to penetrate and the object is placed at a short distance.