Sounders FAQ

Configurations Material

Location of hole in the top of each product is not fixed for PKMCS/PKLCS series. Is it a defect?

This is not a defect. The location of open hole is not specified.
The Open hole is located in one place of 4 corners.
4kHz (The item starting with PKLCS4) do not have a hole in the top.
PKMCS/PKLCS