PTC Thermistors (POSISTOR) FAQQ[PRF Series] What are the conditions for soldering the PRF series with soldering iron?

A

Please note the following points when soldering using a soldering iron.
After sufficient preheating (150°C for 1 to 2 minutes.), use a trowel with φ3mm or less and 30W or less, and solder within 5 seconds at 350°C or less. Use a flux of 0.1wt% or less of halogenated substances. Also, please do not touch the ceramic body directly.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.