Chip Ferrite beads BLM21SN/BLM31SN series supporting 8.5A/12A lines

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

1/2/2016

Chip Ferrite beads BLM21SN/BLM31SN series supporting 8.5A/12A lines

Overview

When it comes to chip ferrite beads for use in power supplies, one major criteria for their selection their high rated current value.

As such, Murata Manufacturing Co., Ltd has added chip ferrite beads that boast 8.5A and 12A ratings in the 0805 and 1206 chip sizes.

  

Background

Chip ferrite beads are used for either signal lines or power lines.

Of these two, when it comes to using the beads for power lines, the rated current value of the beads is extremely significant as an indicator that determines whether they can indeed be used. The maximum rated current value supported by conventional chip ferrite beads in the 2.0x1.2mm and 3.2x1.6mm sizes has been 6A.

By optimizing both materials and internal structure, Murata has now added chip ferrite beads with ratings of 8.5A and 12A to its line-up, thus extending the range of the products’ applications.

  

Features

Despite the small chip sizes of 0805 and 1206, the new chip ferrite beads successfully achieve the high rated current levels of 8.5A and 12A.

  

Applications

For suppression of noise in power lines

  

Parts List

  Applications   Parts List
 For general applications
 BLM21SN300SN1 (0805 size)
 BLM31SN500SN1 (1206 size)
 For automobile powertrain safety applications  BLM21SN300SH1 (0805 size)
 BLM31SN500SH1 (1206 size) 
 For automotive infotainment applications  BLM21SN300SZ1 (0805 size)
 BLM31SN500SZ1 (1206 size) 

  

Production

Mass Production 


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter