Inductors FAQQWhen a board is created by balancing the choke inductor of the RF power supply with the current capacity, the area of the inductor on the board increases, making it difficult to create a compact design. Do you offer an SMD inductor that supports a large current with a compact design suitable for the RF power supply?

A
We recommend the LQP03PN series, which supports a large current and has a size of 0201, as the RF power supply choke circuit.


Related links

The LQP03PN Series


We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.