AMR Sensors FAQQWhat are the advantages of magnetic sensors?

A
  • Magnetic force lines are invisible.
  • Magnetic force lines are not absorbed by plastic, aluminum, copper, and other non-magnetic bodies and pass through to the opposite side. Magnetic sensors use these features to enable detection.
    The advantages can be easily utilized in the following usage situations:
    • Notebook computer open/close detection and security device activation settings (Switch location is not visible.)
    • Gas, water, and other rotation detection (structures where sealing is important)
    • Power switches of wearable devices (the sensor unit requires current, but the sensor is easily adaptable into a waterproof structure)

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.