Inclinometers FAQQWhat is the stability of offset calibration accuracy in the SCA61T inclinometer?

A
Maximum offset calibration error in room temperature is ± 5mg and typical value is ± 2mg (stable) and typical drift is 1mg after 500 hours of having power connected to the inclinometer. Non-repeatability (hysteresis) is 0.25mg when cycling temperature.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.