Ultrasonic Sensors FAQQIn double-feeding detection, high levels of noise are generated, reducing the S/N ratio. How can this noise be reduced?

A
Wrap copper film 0.2-0.3mm in thickness around the sensor and connect the film to the GND of the circuit.
Alternatively, increase the peak-to-peak voltage of the drive signal within the tolerable range to raise transmission sound pressure.
Increasing the number of drive waves may destabilize oscillation and disturb sound waves, resulting in lower sensitivity. Avoid driving the sensor with 6 or more pulses. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.